Part Number: TPA3255
Good day. I am designing a power amplifier based on TPA3255.
The following issues occurred:
The voltage at pin 11 varies in the range of 2.5-3.3 volts.
With the increase of the signal level in the speaker system there is a crack. The power supply voltage is currently 24 volts. Distortions are visible in the photo, with about 6 dB remaining before clipping.
The wiring diagram is fully consistent with the documentation on the chip.