Other Parts Discussed in Thread: PCM5242, PUREPATHSTUDIO, PCM5142, SRC4392
Hi,
I am examining the use of PurePath and the TI PCM5252 DAC for use in a 3 way active speaker project.
The PurePath technical documentation is quite lacking in what is available, so I have requested to access the software to see how it functions and the capability.
In the interim, I am examining the use of the PCM525 as the DAC to be used for each loudspeaker driver path, and as a volume control.
Since the speaker system is an active 3 way design, then I will require 3 Stereo DAC IC’s. Each DAC IC will implement either the low frequency, midrange frequency, or high frequency signals.
Until I obtain the software for Purepath, I am unable to determine if the miniDSP on the DAC can implement the required filter – a Linkwitz-Riley 4th order low pass, or bandpass, or high pass. In addition, I may wish to implement some form of equalisation in the bass path.
The questions I have are as follows :
-
For the PCM5252, page 0, register 61 and register 62 are the digital volume control registers. Are these registers directly writeable and directly readable ?
-
Can the PCM5252 remember the volume setting after a power down ?
-
Can one ensure that upon power up, that the DAC’s IC’s are muted and that a microcontroller can then apply the last used volume setting ?
-
Can the PCM5252 miniDSP programming be used to implement a low pass filter, band pass filter, high pass filter, all 4th or 8th order Linwitz-Riley ??
-
Can the PCM5252 miniDSP implement a delay to compensate for the speaker time delay for the specific drivers physical offsets related to the driver sound focal point transmission ?
-
What are the limits of the delay possible (if possible) in the miniDSP, if the output sample rate of the PCM5252 is 192kHz or 176.4kHz ???
-
If the output sample rate is either 176.4kHz or 192kHz, can the delay be selectable, such that delay1 is used for 176.4kHz and delay2 us used for 192kHz ???
If the PCM5252 can implement the filters, delays, and volume control, then this solution is much more efficient that using a DSP Core and DAC IC’s.
Thanks and regards,
Richard.