Other Parts Discussed in Thread: LM48560, TAS2562, TPA2100P1
Can we connect Electromechanical audio transducer to audio amplifier.
The specification of the transducer is
RATED VOLTAGE 12 Vpk
OPERATING VOLTAGE RANGE 8 ~ 14 Vpk
RATED CURRENT (MAX) 55 mA
COIL RESISTANCE 120 OHM
MINIMUM SPL @ 10 CM (@ 1kHz) 85 dBA
RESONANT FREQUENCY 1,000 - 1,500 Hz
We have connected 3.3V/5V to supply voltage of the IC
I am looking for an audio amplifier that can drive this audio transducer.
Thanks
regards
Subramani