This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TLV320AIC CODECs: Can I drive high impedance loads with a headphone amplifier?



Can I drive higher impedance loads with a headphone amplifier that the impedances specified in the datasheet?

  • It is ok to drive higher impedance loads and, in general, should give better performance than lower loads such as 16-ohms. Actually, this is a good opportunity to place an RC LPF to remove high frequency noise assuming that the load is of sufficiently high impedance that the gain error is negligible. As an added bonus, this also 'isolates' the internally compensated amplifiers from direct capacitve loads. See http://www.ti.com/litv/pdf/slaa313 for resistor/cap values.