Both 5751 operate in PBTL mode and the register configuration is identical.
If the PWM output of the 5751 is not simultaneous, additional power consumption will be generated.
I want to know if the PWM output of the two 5751 is at the same time?If not, what is the maximum time error?