This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5766M: reset timing

Part Number: TAS5766M


Hi TI,

Figure 32 in rev D of the TAS5766 data sheet shows an internal power-on reset signal that must expire > 4ms after the I2S clocks are applied. I have several questions about this:

  • How long does the internal reset pulse stay active after 3.3V is in tolerance?
  • Does the part need all three I2S clocks (SCLK, BCLK, and LRCLK) or just SCLK to be operating when the internal reset is asserted?
  • If I execute a software powerdown (via page 0, Register 2, bit 0 set to 1), does this do the same function as the power-on reset? 

Thanks in advance for your help,

Mike