Other Parts Discussed in Thread: INA1651
Hi
Can i using external resistor to In+ and In- to further reduce the gain ? ( as shown below).
And will there be any impact to the audio quality?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi PYTsai,
As Kai mentions, this is not recommended. Even small mismatch between R126 and R130 in your schematic will significantly degrade CMRR of the INA137. A better solution might be to use a line receiver with buffered inputs, such as the INA1651, and add a "pi" attenuator at the input, as shown:
In this case, because the input impedance of the INA1651 is very high, small variations in R1 and R4 do not have as much impact on CMRR of the circuit. I selected 499Ω and 100Ω resistors to give a 20dB attenuation, approximately the same as your circuit using the INA137, however, these could be increased to 4.99kΩ and 1kΩ to reduce loading on the source.