This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5122: SCK pin configuration with Clock Slave Mode(3-Wire PCM) and resister setting of internal clk

Part Number: PCM5122


Dear Specialists,

My customer is considering PCM5122 with 3-Wire-PCM and has a question.

I would be grateful if you could advise.

---

I have questions regarding the datasheet P.47 8.3.6.3 Clock Slave Mode with BCK CLK PLL to Generate Internal Clocks (3-Wire PCM).

In this case,

(1) SCK pin doesn't use.

Could you please let me know where to connect, GND, VDD, or other ?

(2) I think Internal BCK uses for PLL source, 

When I use fs=48kHz and BCK=3.072MHz, can I set the resister by using Table 131 of fs=48 and SCK=3.072.

---

I appreciate your great help in advance.

Best regards,

Shinichi