Team,
Customer found EMI issue on TAS2557. Below is the current SCH without output LC. When windows volume incresae to higher than 20%, EMI test will fail. Below is the test result of 20% volume. Do you have any advice of how to improve this?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
Customer found EMI issue on TAS2557. Below is the current SCH without output LC. When windows volume incresae to higher than 20%, EMI test will fail. Below is the test result of 20% volume. Do you have any advice of how to improve this?

Thanks Ivan. I will ask customer to try that value. Could you let me know how to enable SSM in PPC3 or registers?
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/6/combined_5F00_configuration_5F00_0_5F00_TuningMode_5F00_48KHz.7z
Hi Ivan,
Attached is the configuration file that was dumped from PPC3. Could you let me know where and how to add "the internal oscillator must be used to generate the ramp, this is done by writing 0x00 into B100_P0_R40. Then SSM mode can be enabled writing 0x01 into B0_P0_R40." to this file? Just to make sure that it is correct. Thanks.
Hi Nic,
Ramp clock is selected in line 10506 as shown in the below capture. The current value is 0x80 which is "PLL". You must change this to 0x00 so that is selects "Internal" instead.
SSM_EN register is not included in the cfg, however you can add a line to enable Spread Spectrum Mode.
The necessary changes are like below capture of the cfg you provided:
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators