This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM386: LM386 Output Power - min<typ?

Part Number: LM386


In the LM386 datasheet in the revision C from May 2017, page 4 states for the LM386N-4:

Pout min == 700mW

Pout typ == 100mW

Is this an error in the datasheet? I am bit confused why Pout min is less than Pout typ. Maybe Pout typ is actually 1000mW ?

  • Hi, Christian,

    Welcome to E2E and thank you for your interest in our products!

    The POUT typ must be 1000mW as you mentioned. We will work to have this corrected as soon as possible.

    Thank you for your observations. They are really appreciated.

    Best regards,
    Luis Fernando Rodríguez S.