This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Our current sensor is easy to be influenced by EM waves in some frequency points, and its OPAMP is RC4580. But I tested out that its EMIRR is above 50dB in 10MHz-1GHz, so it shouldn't come out Dozens of millivolt in the output port. So I want to ask if TI can share the EMIRR test report of RC4580 and OPA2134? and to make a study of EMIRR, I also want to know which OPAMP is not EMI robustness because I want to know magnitude of the offset shift caused by EM waves.