Hi sir
we use the TAS5805M design as PBTL module by output poiwer 40W, PVDD=22V,however, we find the output power only reach 30W,if more than 30W it will happen shutdown, in the datasheet the output power is 45W under the condition of PVDD=21V 4ohms THD=1%, pls help check it and give same suggestions how solve it,tks!