This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am creating a device that vibrates the 6 strings of a guitar. Let me explain what I have working, then let me explain why I need something better. From the output of the guitar's magnetic pickup, I "Yed" the guitar's signal to a OPA134, arranged as a non inverting op amp with gain. The output of the OPA134 then went to a LM386 set to the maximum gain of 200. The LM386 was originally designed to drive a 8 ohm speaker. The output of the LM386 is what drives the "things" that vibrates the metal guitar strings. Ok, what are those "things" that vibrate the guitar's metal strings? The "things" are 490-CEM-1203(42) magnetic buzzers. I removed the top half of the buzzers, the part that made the noise. This left only the bottom half of the magnetic buzzer, which contained the magnet, with copper wire wrapped around the magnet. If you run current through copper wire wrapped around a magnet, you create a electromagnet. By now you should be getting the point. Meaning the guitar's sine wave signal activates the tiny electromagnets laying close under the guitar's steel strings.
It seems to work best when there are two of these tiny magnetic electromagnets under each string, especially the smaller strings. Each of the tiny magnetic electromagnets are 42 ohms. I selected 42 ohm values for a reason. That reason was to try and match out the ohm value of the output of the LM386, which is 8 ohms. I connected the 42 ohm tiny electromagnets all in parallel. This means 4 of the 42 ohm tiny electromagnets in parallel had a ohm value of 10.5 ohms. 6 of them in parallel had a ohm value of 7 ohms. This means we are already below the 8 ohm design of the LM386. Therefore, if we put 12 of the tiny 42 ohm electromagnets on the guitar, in parallel, we have a total ohm value of 3.5 Ohms. The LM386 was not designed to drive a 3.5 ohm load.
Possible solutions: Hooking up two of the LM386 power amps, each driving half of the load. That seemed like the easy way out. I then tried another approach for the electromagnet part of the device. A guitar's pickup is wound with approximately 40 AWG magnet wire, to ohm values ranging from 10K ohm to 20K ohms. I removed the original magnet wire from a guitar's pickup, then wound new 32 AWG magnet wire around the magnets, until I got a 8 ohm reading. This did work, and did vibrate the strings, but did not vibrate the strings as strong as I would like. The distance the guitar strings are away from the electromagnet field determines how strong the magnetic field needs to be. To me this meant the LM386 was not putting out enough current, to create the magnetic field vibration I wanted. This led me to think I needed a amp more powerful than the LM386, and that would require searching. The other problem involved with finding a new and more powerful amp, is finding one with suppression diodes. Any time a magnetic coil collapses current can flow in reverse. So a new amp would have to be a audio amp designed to drive a speaker. A small audio amplifier with one input, and one or two outputs.
Then I started thinking outside the box. Meaning there should be a totally different and better way to vibrate the strings. I thought of using a transformer to match the ohm values, but that idea seemed to draw too much current. Maybe I am wrong about too much current. I also thought of creating a stronger single electromagnet, but that also required more current. Then I happened upon a idea that seemed good. I read data sheets on TI's Darlington Transistor Arrays. If I could only bias the 7 inputs of the Darlington Transistor Arrays from the output of the OPA134, this would provide everything I thought I needed. Then I find that the ULN2002A has a 7 volt zener on the input, and was designed for P-MOS switches. The other two similar arrays ULN2003A and ULN2004A are designed as switches for TTL and CMOS devices.
At this point, I am dead in the water, and it is not a good feeling! I would like some suggestions on how I can better accomplish controlled string vibration? Thanks Keith Hilton