This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5825M: TAS5825M edge rate control

Part Number: TAS5825M
Other Parts Discussed in Thread: TAS5782M

Hi professional,

I heard that Edge-Rate Control of TAS5825M is optimized for trade off between dead-time and EMC.

Our customer's understanding is that TAS5825M has no difference regarding EMI when we compare TAS5825M and the other product which doesn't support filter free operation if we don't use TAS5825M's channel to channel phase shift. Is this understanding correct?

I'm looking forward hearing back from you.

Best regards,

Kazuki Kuramochi

  • Hi Kazuki,

    1. I heard that Edge-Rate Control of TAS5825M is optimized for trade off between dead-time and EMC.
    Yes, if edge-rate is optimized, then EMC would be better, while dead time could be a bit longer. It depends.

    2. Our customer's understanding is that TAS5825M has no difference regarding EMI when we compare TAS5825M and the other product which doesn't support filter free operation if we don't use TAS5825M's channel to channel phase shift. Is this understanding correct?
    EMI is quite complex, quite a lot thing can be optimized to reach better EMI, including edge rate, phase shift and PWM modulation, FET design. Each product have different EMI features with different design. If customer can have accurate product-product comparison(TI device), we may able to do a general EMI comparison.

    Dylan
  • Hi Dylan,

    Sorry for my late reply.

    As a conclusion, TAS5825M has better EMI performance than the other Mid power Audio AMP that has similar function even if TAS5825M's channel to channel phase shift is disable. The reason is TAS5825M optimized edge rate, layout, etc. Is this correct?

    Thanks,
    Kazuki Kuramochi
  • Hi Dylan-san,

    Would you provide your feedback for this?

    Thanks,
    Kazuki Kuramochi
  • Hello Dylan-san,

    Our understanding for TAS5825M is that TAS5825M has better EMI specification than the other D-AMP(ex. TAS5782M) even if TAS5825M don't use channel to channel phase shift. Is this correct?

    I'm looking forward hearing back from you.

    Thanks and best regards,
    Kazuki Kuramochi
  • Hello Dylan-san,

    Your early reply will be greatly appreciated.

    Regards,
    Kazuki Kuramochi
  • Hi Kazuki,

    There is advanced spread sepctrum modulation, channel to channel dephase, and also optimized edge rate control during ATE trim stage.

    As Dylan mentioned, EMI is highly related to test condition setting. Could you share the 'same performance' data to us?

    Rdgs,
    Matthew
  • Hi Matthew,

    Thank you for your reply.
    I received answer by the other internally discussion.
    So I closed this question.

    I appreciate your team's support.

    Regards,
    Kazuki Kuramochi