Other Parts Discussed in Thread: TLV320AIC3101
Hi all
Would you mind if we ask TLV320AIC3100?
It seems that headphone outputs(HPL/R) are inverted against inputs..
The conditions are follows;
INPUT : MIC1LP only with single end
OUTPUT : HPL/R, the setting is lineout driver(P1R44[D2-1])
So, is there any un-inverted setting using register?
In addition to this, TLV320AIC3101(headphone outs(HPLPUT/HPROUT) had the same problem.
As the result of this, mixer circuit after DAC inverts signal.
Kind regards,
Hirotaka Matsumoto