Hi,
My customer would like feedback to their tests:
"We tried to do some testing with our supplier on the TPA3221 evaluation board with 16.8V Vcc, 2ohm resistor load, BTL. 1KHz signal.
It seems that the peak voltage we measured at the speaker output is about 14.5V.
I scan in the spec, there is no Plimit setting, I would expect the peak voltage to be close to 16V.
Is this normal to have 14.5V as we have measured ?
We are still 2A away from the OCP of 10A and we would need just a few cycle of peak power.
1) Please confirm if our finding is correct.
2) Also, would you be able to share the efficiency curve for 16V, 2 ohm, BTL configuration ?"
Thanks for looking into this, and maybe suggest alternative output inductors to use on the EVM.
B.r M.A.M