This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM48511: Can it accept PWM inputs instead of "pure analog sine wave" from a microcontroller ?

Part Number: LM48511


Since many microcontroller has PWM outputs, if LM49511 can support PWM inputs, then then design will be much more efficient. 

  • Hi Jerry,

    You can use a PWM as input signal, however you must place a Low-Pass Filter between PWM output and LM48511 input.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators
  • Hi Ivan:

    I notice that LM48511's inputs are all AC coupled, in this case, if I feed in two PWM signals to them, should they be ok?

  • And by the way, Ivan, which ground should the thermal pad connect to ? In the datasheet of the chip, it suggests that this thermal pad should be connected to the signal ground, i.e, GND2, but in the demo board user guide (AN-1922), the thermal pad seems to be connected with GND3, which is the ground of boost converter. which senario should I follow? Thanks, Jerry
  • Jerry,

    If input signal is a PWM it still needs low-pass filter. AC couple would remove the DC bias, however it will most likely continue being a square-wave signal.
    Regarding the thermal pad, you should solder this to GND plane for dissipation purposes. In the case of the EVM it is not connected on the top layer to any of the GND pins, layer 1 is used for GND2, layer 2 is used for GND1 while bottom layer is used to connect all GND1, 2 and 3, as well as thermal pad.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators
  • Thanks for your answer, Ivan.

    I'm just wondering, will the sigma-delta control loop of the class D amp filter out these high frequency stuff in PWM? I didn't find any information about the bandwidth of the loop in the datasheet.

    If you can provide several insights on this subject, it will be awesome!

    Thanks, Jerry

  • In the application document, it uses 4-layer PCB configuration, is 2-layer configuration acceptable?
  • Jerry,

    2 layer board would be OK.
    This is an analog input device and it is not meant to be used with PWM-like signals. As mentioned before, if this is needed an external low-pass filter must be placed at the inputs. Unfortunately there is not much more information available that can be shared of the internals of the device.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators