This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS3251: Standby mode power consumption reduction plan

Part Number: TAS3251


Dear Support team,

Our customer will use TAS3251 in their application.

They are designing supply circuits that are their product's standby.
If they use below conditions, is their has any problem?

 GVDD_A / GVDD_B : 12V
 PVDD_A / PVDD_B : 24V
 DAC_DVDD / DAC_AVDD : 0V

And, do you have any conditions or timings when supply pow-ON/OFF?
When they use always PVDD/GVDD ON , it will be controlled only DAC_DVDD/DAC_AVDD.

Best Regards,
Hiroaki Masumoto