This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PUREPATH-CMBEVM: PUREPATH-CMBEVM

Part Number: PUREPATH-CMBEVM

My customer bought PUREPATH-CMBEVM

Our part No: 2379251

Please find my customer query.

The device connected through USB is not recognized. Is this problem you are facing?

It comes up as Unknown device in the device manager. It should come up as an Sound device.

It was working yesterday but not this morning.

Operating System: Win 10

I've tried multiple cables and two computers without success.

And also need user manual for this.

Please help to solve the issue