Part Number: OPA1652
Hi all,
I am using the OPA1652 (WSON8 package) in gain=1 configuration with +/-15V supply, and it gets quite hot; app. 40°C above ambient with idle input.
When I apply a 400kHz sine signal with +/-10V amplitude, the top case temperature is app. 60°C above ambient.
I wonder if this is ok for operating the OPA1652 at am ambient temperature of +85°C, since it will result in 145°C top case temperature.
I think that the junction temperature will be app. 150°C in this case.
Is this ok?
I searched the data sheet and found several temperature ratings, but not the one I need.
On Page1, there is no iformation about the kind of temperature (case, ambient, junction, ...):
On page 5, I get information about the absolute ambient and junction temperatures,
and the recommended operating ambient temperature:
At last, page 7 lists two temperatures, but does not show what kind of temperatures (Junction, case, ambient) is meant:
So back to my question:
What is the recommended operating junction temperature range for the OPA1652?
Regards, Niels