SCH-WSS_BM20L-V02.pdfTPA2080D amplifier problems are as follows:
1, when the volume is up to the maximum, the distortion is relatively large
2. When the volume is up to the maximum, the IC works very hot
3. When the volume is up to the maximum, the output of the amplifier is unstable