This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1678: Noise Simulation

Part Number: OPA1678

The OPA1678 noise is spec'ed for 4.5 nV/sqrt(Hz) at 1 kHz.

Using the following circuit in TINA, where the VG1 source = 0V,

and performing Analysis->Noise Analysis->Total Noise returns this result:

I expected this value to be closer to 4.5 nV * sqrt(1000 Hz) = 126 nV.  

Using the Analysis->Noise Analysis->Input Noise returns,

Which also returns a value higher than expected.

Can you please let me know what I'm doing wrong here?  Is it related to the Flicker Noise of the device?

These noise voltages are RMS, as confirmed by simulating the noise of plain resistors.

Thanks, Best, Steve

  • Hi Steve,

    Thank you for your post. When you are calculating op amp total noise, you have to take into account both broadband and 1/f total noise. The formula you have will only apply if the broadband noise extended across the entire frequency range. But since the OPA1678 does have a 1/f component, this needs to be included. The Analog Engineer's Pocket Reference guide goes over these formulas / calculations on pages 61-62 (https://www.ti.com/seclit/ml/slyw038c/slyw038c.pdf).

    In regards to the second curve for input referred noise, this is a slight error in the model but expected. The model mimics the datasheet parameters closely but it isn't necessarily exact. 

    -Tamara