Other Parts Discussed in Thread: TAS5805M, , TAS5825M, TAS5805
Dear Sirs,
My customer asked us about comparison of the parameter settings (at startup) of the TAS5805M .
He compared the parameter settings (at startup) of the TAS5805MEVM using PurePathConsole3 in the following two ways.
1. Output header file using header file output function
2. Log at parameter setting with I2C monitor log function
Then he found some unknown sub addresses and data.
Please let us know about the following unknown Sub Addresses and Data.
Both of Header File and I2C Monitor LOG File
a)
Book:0x00 Page:0x00 Sub Address:0x7D
⇒cannot find description this sub address
b)
Book:0x00 Page:0x0 Sub Address:0x7E
⇒cannot find description this sub address
c)
Book:0x00 Page:0x01 Sub Address:0x51 Data:05
⇒Why is it the setting only for Right Ch?
d)
Book:0x00 Page:0x01 Sub Address:0x66 Data:87
⇒87 means bit7=1 but this bit is reserved
e)
Book:0x8C Page:0x2C Sub Address:0x74
⇒0x74 is not in the register map in Page 2C
f)
Book:0x8C Page:0x2E Sub Address:0x24
⇒0x24 is not in the register map in Page 2E
g)
Book:0x8C Page:0x32 Sub Address:0x08
⇒0x08 is not in the register map in Page 32
Also Page 32 is not register map in 0x8C
h)
Book:0x8C Page:0x33 Sub Address:0x08
⇒0x08 is not in the register map in Page 33
Also Page 33 is not register map in 0x8C
i)
Book:0x8C Page:0x34 Sub Address:0x08
⇒0x08 is not in the register map in Page 34
Also Page 34 is not register map in 0x8C
j)
Book:0x8C Page:0x35 Sub Address:0x08
⇒0x08 is not in the register map in Page 35
Also Page 35 is not register map in 0x8C
k)
Book:0xAA Page:0x2E Sub Address:0x7C
⇒0x7C is not in the register map in Page 2E
l)
Book:0xAA Page:0x2F Sub Address:0x08
⇒0x08 is not in the register map in Page 2F
Also Page 2F is not register map in 0xAA
m)
Book:0xAA Page:0x2F Sub Address:0x1C
⇒0x1C is not in the register map in Page 2F
Also Page 2F is not register map in 0xAA
I2C Monitor LOG File Only
n)
Book:0x8C Page:0x2D Sub Address:0x08
⇒0x08 is not in the register map in Page 2D
o)
Book:0x8C Page:0x2D Sub Address:0x0C
⇒0x0C is not in the register map in Page 2D
Also Are there any plans to update the document?
Best Regards,
Y.Hasebe