Other Parts Discussed in Thread: TAS2770, TAS2557
Hi
Can you suggest the speaker amplifier for the following requirement
1. Minimum 5W amplifier
2. Class D amplifier
3. 1-Channel (Mono)
4. Real-Time Diagnostics Using I/V Speaker Sense
5. Digital input - I2S interface and I2C
6. Protections - Over Current,Short Circuit (short to power, short to ground and terminal-to-terminal short), Over-Temperature
7. Shall detect open and short condition
8. Power supply maximum PVDD - 23V
9. IOVDD - 3.3V
Thanks and regards,
R.Sivasuryan