This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2557: Audio noise when Vsense enabled

Part Number: TAS2557

With IV sense function disabled, customer's system worked well.

WIth IV sense enabled, customer observed noise at these frequencies:

- 2.4Hz (Large amplitude swings, leading to audible amplitude cycling at 2.4Hz)

- 58.5Hz (constant humming)

- 125KH & 180KHz (no issue, not audible, just for info only)

This was measured using 8KHz sampling, 1KHz test tone, BCLK = 1.536MHz.

What can cause such type of noise to be introduced, only when IV sense is enabled?

- I have schematics, scope captures, layout available for offline discussion.