Part Number: TAS2557
Hello!
I have the following setup: A TAS2557EVM with PurePath Console 3 and a TAS2557 device embedded in my own breadboard. The embedded TAS2557 device is using I2C and is hooked up with the I2C-probes on the EVM-board. My embedded TAS2557 is using 22050Hz, 16bit and is acting as a master on I2S.
I am able to generate configuration files when dumping the binary file, but I am not able to generate header files for my embedded program. Is there a way to setup my embedded TAS2557 using TAS2557EVM and PurePath Console 3, and also generate header files instead of .cfg-files, which I have to manually type as I2C commands in my embedded software.
I would also like to use PurePath Console to tweak some parameters and listen to the changes on my embedded device. And when im satisfied with the result, empty the configurations and save as a header file, Is this possible?
Thank you in advance,
/Viktor