This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2557: Noise when using low sample rates

Part Number: TAS2557

Hello!

I am using TAS2557 working as a master on I2S (WCLK 22050Hz, BCLK 705600Hz). When playing a 22050Hz/16bit sound file there is a noise added to it. But when i convert the same sound file to 44100Hz/16bit and change WCLK to 44100Hz and BCLK to 1,4Mhz it sounds much cleaner and louder.
I have generated a .cfg file from PPC3 for 44100Hz (since I could not generate a 22050Hz) and configured it for 22050Hz my self. But is there any other configurations I need to have in mind when lowering the sample rate in order to reduce the noise?

Thank you!
/Viktor

  • Hi Viktor,

    In order to configure the device to 22.05kHz sample rate some registers that are not currently shown in the datasheet must be changed. Usually these registers are calculated within PPC3, but as 22.05kHz is not one of the options this must be made manually.
    Let me create and test a script for this configuration and I'll share it with you.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

  • That would be great!
    Thank you, Ivan.

    /Viktor

  • Hi Viktor,

    22.05kHz sample rate is not supported on this device, as you can see in Book 0, Page 0, Register 0x2F (Table 50).
    The supported sample rates are 8k, 16k, 48k and 96kHz.

    Do you want to use the device in tuning mode? You can configure the device to any of these sampling rates using PPC3 end system integration panel.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

  • Hello Ivan!

    Alright, good to know!

     
    The configuration file for tuning mode is quite to large for our embedded application, so we are probably going to use ROM Mode 1 or 2. The sampling frequencies supported by the PPC3 end system integration seem to be 8k, 16k 44,1k and 48k. So I figured that we could use 22.05k since it is a multiple of 44.1k.

    Thank you for your help!
    /Viktor

  • I also noticed that in ROM Mode 1/2, PPC3 end system integration only support 44.1k and 48k.
    Is there any settings that I need to apply besides WDIV and BDIV ratio to make the device support 22050Hz?


    It seems most logical that you can choose 44.1k or 48k with PPC3 and then use some divider to use a multiple of that sample rate for the device. Because the datasheet states that in ROM Mode the device supports sample rates from 8kHz - 96kHz, with a maximum of 48kHz when using speaker protection.

    /Viktor

  • Viktor,

    The clock dividers might be able to set 22050Hz, but Register 0x2F from Book 0, Page 0 does not have this sample rate as an option.

    ROM mode supports lower sample rates, same as Tuning mode, even though PPC3 only shows 48k and 44.1k options. If you need 8k or 16k rates in ROM mode please let us know and I can provide a cfg file for these rates and your specific source clock.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

  • Ivan,

    I tried configuring the device for 48kHz/16bit and played a 48kHz/16bit audio file and the sound was clear and crisp.
    Then i tried to configure the device for 16kHz/16bit, changing register 0x2F as well as changing the BDIV/WDIV to the correct frequencies, and played a 16kHz/16bit sound file. The sound was just as noisy and unclear as it was when i played using 22.05kHz/16bit.

    So is there nothing else than changing register 0x2F and BDIV/WDIV?

    I compared the configuration files between 44.1kHz/48kHz and noticed that there are some changes in registers not shown in the TAS2557 datasheet:
    1) Book: 0x64, Page: 0x00, register: 0x1c 
    2) Book: 0x64, Page: 0x00, register: 0x1d
    3) Book: 0x64, Page: 0x00, register: 0x1e
    4) Book: 0x00, Page: 0x32, register: 0x54 - 0x57

    Do you have any documentation regarding these registers?

    I also noticed an existing thread regarding my problem which sadly has been locked due to inactivity by the poster, but would be interesting to get an answer to:
    https://e2e.ti.com/support/audio/f/6/t/718459?TAS2557-Asking-for-the-TAS2557-sampling-rate-support

    Thank you Ivan,
    /Viktor

  • Viktor,

    The clock source goes through some divider/multiplying stages, additional to register 0x2F.

    1) Book: 0x64, Page: 0x00, register: 0x1c                  PLL J multiplier
    2) Book: 0x64, Page: 0x00, register: 0x1d                  PLL D multiplier (MSB)
    3) Book: 0x64, Page: 0x00, register: 0x1e                  PLL D multiplier (LSB)
    4) Book: 0x00, Page: 0x32, register: 0x54 - 0x57       This book and page correspond to the program memory

    Currently there is no public documentation that shows further detail on device clock configuration, but in the meantime you can provide the following details and we can send back a cfg file:

    • Clock source: BCLK or MCLK
    • Clock source frequency: Same as options shown in PPC3 for BCLK or MCLK
    • Sampling frequency: 8k, 16k, 48k, (96k just for ROM modes)
    • Mode: ROM1, ROM2, Tuning

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

  • Okay, thank you!

    Clock source: MCLK
    Clock source freq: 12MHz
    Sampling freq: 16k
    Mode: ROM1
    Also, we are using I2S where TAS2557 is master, thus generating BCLK and WCLK.

    If possible, could you please create a cfg-file for both 16k and 8k sampling frequency?

    /Viktor

  • Hi Viktor,

    Attached is a script that should work for the following:

    • MCLK = 12MHz input clock
    • Sampling rate 16kHz
    • ROM Mode 1
    • Master (BCLK and WCLK as outputs, derived from MCLK)

    Could you please try this on your side? Currently I'm not able to test with a MCLK = 12MHz that can send 16kHz sample rate data. Although I'll try this as soon as possible.

    If this works fine, then I can provide 8k cfg as well.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

    48k_12M_MCLK_ROM1_Master.cfg

  • Hi Viktor,

    Did you got a chance to test the attached script on your side?

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

  • Hello Ivan!

    I apologize for not informing you, but i simply changed Book 100, page 0, register 1b from 0x01 to 0x02. The frequencies came out correct and the audio sounded clear and I think that I am satisfied with the configurations for now. 
    Thank you for all your support, Ivan.

    /Viktor