This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3256: TLV320AIC3256 configured as I2S , ADC sample well but DACs are not response

Part Number: TLV320AIC3256


I use the codec IC  with I2S audio interface.for the ADC - IN3  and DAC - LOL and ROL.

the IC is initialized as secondary  I2S slave  with BCLK and WCLK  provided to the codec by the host controller of the codec.

the ADC_CLK is provided by the inserted BCLK  (500KHz)  and the PLL that multiply the BCLK by 4 (2MHz) to provide the ADC_CLK,  instead of the MCLK (as was with the Evaluation board).

I saw that the DI and DO of the secondary  I2S of the codec including the BCLK and WCLK (8KHz) are  as expected.

I insert a signal to left  ADC and right ADC and I could see the sampled data 16 bit of each channel seems to be properly and as expected but when we sent data (even constant data) we could not see the analog signal on the DACs LOL and ROL  output as refer to the sent data. All we could see on the DACs output  was noise (seems to be random) with amplitudes that were even reach the maximum allowed amplitude.

As told we don't use and not insert MCLK to the codec.

the question is what we are missing so the DACs LOL and ROL analog signal output is not according the data that is sent to the DACs (via DIN) and instead we receive large noise?

Is the inserted  BCLK of the I2S  is a sufficient CLK signal in order to enable also  the DACs to work according the data that is sent from the I2S? 

If required I can send the registers init   values  as configuration via the I2C interface.

 

Thanks,

Kobi