Part Number: OPA1602
I used the tidu035crossover as a starting point and then modified the design to build a single low pass filter with the signal path as follows: I started with the same unity gain buffer stage and 10k input resistance, then two Sallen-Key filters (2nd order Butterworth alignment @ 300Hz) followed by a unity gain buffer stage. The unity gain stage is direct coupled from the filter stage. Input is 1V P-P 20Hz and the power supply is +/-12V.
The output is clipping and refuses to go below zero volts on two out of four of these circuits that were built. The other two work fine. I tried adding a 1k resistor to feed the buffer but I still get clipping.
The problem is in the buffer stage... what is going on here?
Thanks for you help!
Bob