Hi, I have a MCLK of 12MHZ and incoming data on I2S at 16KHz sample rate (fs). What would the recommended clock tree look like?
Do I have to create an internal clock that is 256 x Fs ie 4.096MHz DAC ie DAC fs. To get the 4.096Mhz I have to use the PLL as there is not an integer solution.
Can I also ask what the DAC sample rate register does ( page 1 reg 02) in my case is this changing the Fs 0f 16KZ to a lower value that I then have to multiply by 256 to get the correct DAC Fs.