Hi professional,
My customer has question for TAS5825M's FSMODE resister.
Datasheet p48 Table 11. SIG_CH_CTRL Register Field Decrictions said "Need set it manually If the input Fs is 44.1kHz/88.2kHz/176.4kHz".
Is this meaning we couldn't use Auto detection for 44.1kHz/88.2kHz/176.4kHz digital audio signal input and must need to configure FSMODE manually?
Do you have any way to use Auto detection for 44.1kHz series input signal?
By the way, datasheet table11 mentioned FSMODE has 1bit in 0x28 for configuration. However FSMODE need 4bit for configuration. In PPC3, FSMODE has 4bit (3~0) in 0x28.
I think datasheet is typo and PPC3 is correct. Is this right?
I'm looking forward hearing back from you.
Best regards,
Kazuki Kuramochi