Other Parts Discussed in Thread: TPA3138D2, PCM5122
Dear team,
I am working on the design that should include an audio interface with the following requirements:
- It should receive digital audio data from the MCU
- It should have Line out
- It should be able to drive four 1W/8Ohms speakers (every two speakers are connected in parallel per amplifier channel)
I have designed the schematic diagram using mentioned ICs from TI and will appreciate if you can review the connection between PCM5121 and TPA3138D2 as well as the Lineout circuit. The power amplifier will be powered with the fixed 5V, so at the 4Ohms load (two 8Ohms speakers connected in parallel), there shouldn't be more than ~2.5W which is suitable for the used speakers. I will limit volume in order to limit the output power in the firmware.
Please find attached schematic.
Thanks in advance.