Other Parts Discussed in Thread: , PCM1862EVM
HI,
I'm trying to get a response from the 1863 control interface from an ESP32 talking SPI I get no response from the chip. I think I must be completely not understanding how to wire up this chip.
Currently I have IOVDD/AVDD/DVDD tied to 3.3v. AGND/GND are tied to GND. There is a 12mhz crystal on XO/Xi. M0 has a 10k pull-up to 3.3v. The SPI pines (MS/MC/MISO/MOSI) are connected to my micro-controller. SCLKI/BCLK/LRCLK/DOUT are all floating.
Is that a sane configuration?
Also,
(a) Are there any example basic application circuit for a PCM1863 being run by a general purpose microcontroller? Preferably with source code?
(b) Will the PCM1863 respond on SPI if nothing is connected to the I2S channel?
Thanks,
Albert