Part Number: TPA3128D2
Other Parts Discussed in Thread: TPA3132D2,
Is there any way to determine the PLIMIT voltage required other than experimentally? Some of the other parts with PLIMIT have graphs showing PLIMIT vs Max. Output Power,
but the TPA3128D2 only states "The "virtual" rail is approximately four times the voltage at the PLIMIT pin" and Table 3 indicates the ratio of PLIMIT voltage (V) to Output Voltage (Vrms) ranges from 12.67/3.3=3.84 to 6.3/1.5=4.2. Are the units on this table correct with the output voltage Vrms, because he text says the 4x is for Vpeak?
Is GVDD as loosely regulated as the datasheet indicates (5.1V 5.6V 6.3V)? This would translate to a power limit range of -17% to +27% if the nominal GVDD is used for calculations.
In section 6.5 DC Electrical Characteristics,
Does this indicate that the limit may kick in 32% (1-(6.75/8.2)^2) below the nominal power level when the PLIMIT voltage is set precisely? Is this range related to the VCC? The TPA3132D2 datasheet has graphs indicating higher clip levels when the virtual rails are close to the actual supply voltage.
My desire is to design an amplifier using the TPA3128D2 which runs off a higher than needed VCC (24V) and limit the maximum unclipped output power to a guaranteed level (15W). Is this feasible? If I am interpreting the datasheet correctly for G, GVDD, and Vo , I would need to set the PLIMIT at 33W (15/(0.89 * 5.1/5.6 * 6.75/8.2)^2)to guarantee 15W if I use GVDD or 29W (15/(0.89 * 0.99 * 6.75/8.2)^2) if I use a 1% voltage reference. These number do not seem reasonable.
Thanks in advance for your assistance in clarifying the PLIMIT operation.
Jon