Part Number: LM4670
Other Parts Discussed in Thread: LM48511, TPA2013D1, LM4675
Hi,
I am observing a similar issue as https://e2e.ti.com/support/audio/f/6/p/618222/2278402 My PCB layout looks good as shown in this existing thread.
The device output pins Vo1 and Vo2 show below response on an oscilloscope when there is nothing driven from our host processor to IN+ and IN-. CH1 is Vo1 and CH1 is Vo2. Channel M is the math function enabled Vo1-Vo2.
Attached is the schematics and noise recording audio file. The sound is similar to a continuous hiss.
Few observations:
I have tested with a 220Ohm@100MHz ferrite bead in-place of R327 and R328. It helps a bit to reduce the audio noise intensity but makes the graph look worse with lots of overshoots and undershoots. I could still hear the noise without any playback.
Shutting down of amplifier using the pin completely reduces the noise.
While playing the file, the noise goes off and then it restarts after the playback of intended mp3 file duration.