This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3220: Using the internal 5V0 LDO

Part Number: TPA3220

I'm trying to use the internal LDO in the TPA3220 and I must be doing something really silly as I can't get it to work

I am feeding the same voltage to the VDD (pin1) as I am into the PVDD pins - 30V

I have disconnected AVDD and GVDD from the VDD pin 

When I power up I m expecting to see 5V0 on the AVDD (pin 21) but I only get 0V

Is there something else that needs to be done to activate the internal LDO regulator?

Just for the record I also have the recommended filter on GVDD and decoupling capacitors. The chip works fine with an external 5V0 regulator but I was trying to reduce the component count

Thanks in advance