This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5731: TAS5731 DEMO test

Part Number: TAS5731

Hi TI Team:

    When my customer debugging the DEMO board found there are some problems on the output mode Settings,  They want to set a SE output mode, but when set to manual register configuration parameter is different, when 0x05 register setting, should be in accordance with the manual D2 to 1 is the SE model output, but the fact is that when the D6 and D2 both 0, the SE output port can have 2 channel output, when D6 is 0 and D2 is 1, the output SE port only 1 channel, when D6 is 1, there is no output.

    Please check the attachment configuration interface, thanks!

TAS5731模式设置.docx