Other Parts Discussed in Thread: OPA1632
Hi sir
My questions as below.
1. PCM1864 can support XLR interface input(Fully Diff)?
2. If we need add pre-amp in front of PCM1864, OPA1632 is suitable?
Thanks for your great support.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Yes, the PCM1864 can directly acquire differential outputs from an XLR connector. I copied a section from the datasheet below that explains the inputs can be configured as differential or single-ended.
The PCM186x family of audio, analog-to-digital converters (ADCs) features a highly flexible, audio front end that
supports input levels from small millivolt microphone inputs to 2.1-VRMS line inputs. The analog front end can be
configured to support either differential or single-ended inputs, providing optimal performance when using
differential inputs. Mixing single-ended and