This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
We met a problem is , 4-8ohm load is no problem but 2ohm enter to OLP ,would you please take a look and provide the suggestion, thanks you!
In 2ohm Vin=48V , 1K frequency
1.the out pin : FAULT=0,CLIP=1
2.Mode=PBTL ,M1=0 / M2=1,J7/J8=0,OUT A and C shorted,OUT B and D shorted
Output RMS=30V
Hello Anle,
What did you configure your current limit to be for OC Protection. Have you tested the configuration in both pre-filtered and post-filtered PBTL. Also you say Vin is 48V, did you mean your PVDD is 48V?
Best Regards,
Luis