Hi team,
I'm interested in using DIT4096 in an application where the I2S source will be a Bluetooth module. The BT module format may change, but the base mode is as follows:
- BT module = master, DIT4096 = slave
- 16-bit I2S
- BCK = 1.536MHz (32*fs)
- LRCK = 48kHz
I believe only the software-controlled version can support 16-bit I2S. So if we stick with the SW-controlled DIT4096, can it support this application? I believe the answer is yes, but I wanted to get confirmation. Thanks!
Brian