This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1863: THD with 5.5Vpp Input Signal

Part Number: PCM1863
Other Parts Discussed in Thread: , OPA1678, TLV320ADC3140, TLV320ADC5140, TLV320ADC6140

Hi Team,

The single-ended full-scale (FS) input of PCM1863 is 2.1Vrms, now the maximum input of our application is 5.5Vpp which is equal to 1.94Vrms. So the input level is -0.67dBFS, but the figure 6 in the datasheet doesn't show the specific turning point where the THD+N is getting worse.

Unfortunately, I don't have a PCM1863EVM at hand, could you please help confirm the THD+N for -0/67dBFS? Thanks!

Best Regards!

Hao