This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

we need a audio interface IC which can support Inpu LINE x2;S/PDIF x1,COAX x1

Other Parts Discussed in Thread: PCM9211

hello

we need an audio interface IC,  requirements as below:

1. Input:  LINE inx2; S/PDIF  x1; COAX  x1 

2. output:  I2S;

3. can detect the active input port automatically, 

4. sample rate 48k/44.1k; SNR>94dB, 

5. can work in host mode

Please help provide the suitable device, Thanks a lot!