Other Parts Discussed in Thread: TAS5754MDCAEVM, TAS5756MDCAEVM, TAS5825MEVM
Hi - I just finished a TAS5754/6 design and I wanted to do an upgrade with the TAS5806. I'm a bit confused by the filtering looking at the schematics and the EVM.
The TAS575xEVM shows a BTL with 2x22uF on PVDD and a 4.7uH speaker output filtering inductor while the PBTL shows a much larger 390µF on PVDD as well as a larger 10uH inductor, which makes sense.
Now TAS5806EVM shows 2 designs as well, but they both seem to be BTL and one has a set of 2x22uF on PVDD and uses a small ferritebed for output filtering where the other design is a BTL as well but shows a 4.7µH inductor for output and a very large 390µF on PVDD. Meanwhile, the datasheet only shows the 390µF/4.7µH combination
So if they are both BTL, what's the recommendation?
Thanks