This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6422-Q1: Clocks problem

Part Number: TAS6422-Q1
Other Parts Discussed in Thread: SRC4392

Hello,

I'm trying to make the TAS6422 work but there is no way to do it. I think I'm missing something but I saw some user in this forum asking similar question and using same MCLK clock reference.

I have 24.576 and 22.5792 clocks available, somehow I managed to get it working at 44.1kHz but with clock problems, so it does not sound "clear" probably to some clock ratio failure.

Do I need to go down to 12.288 foe example or I can make it work with current clocks for MCLK? In that case, can you point me on the right direction? 

For example I have those clocks now:

- MCLK: 22.579 MHz

- SCLK: 2.8 MHz

- LRCLK: 44.1 kHz

I'm using SRC4392 as data source, I2S output on port B.

Thanks!