Hello support team,
I have some questions regarding PCM3060.
According to the data sheet, it is recommended to generate VDD (3.3 V) from VCC (5 V) for the power-on sequence.
However, in the customer's application, VCC and VDD are generated separately. Therefore, there is the possibility that the power-on sequence may be indefinite.
[Question]
1. In this case, will this IC work normally if the external reset is released after both power supplies have been stabilized?
2. Are there any concerns that latch-up will occur?
Sincerely,
M. Tachibana