Other Parts Discussed in Thread: CC8520
Hi!
I'm building my own little app using the CC8520, really basic mono transmission.
I have a transmitter which is working perfectly, i already tested it with the PPWDK. But i'm having nighmares, literally, with my receiver.
The thing with the receiver is that, i'm testing it with the PPWDK, it has what i think are connection problems with the master DK board. When i get them to connect one of several things happen: (1) the master board connects but after a few seconds it shows the alone blinking pattern, (2) sometimes it shows LED D9 on, as if it was connected but there's no audio tranmission, (3) or sometimes my receiving board shows the standby pattern, (4) even sometimes, my receiving board shows the connected on pattern whilst the master board shows the alone patter, there's no master connected to it!!
Every once in a while after hitting the reset button on my board, the one i had made, it blasts out a second or two of sound, but it goes away as fast as it comes. I have checked it over and over again but i can't seem to find what's wrong... maybe i'm going blind...
I'm attaching the schematic for my receiving board, i would highly appreciate ANY help on figuring out what is wrong!!!
Regards,
Daniel Jimenez