Part Number: TAS2552SW-LINUX
Other Parts Discussed in Thread: TAS2552, TAS2557
Hi,
We've made a custom board with 2 tas2552 codecs which are connected to an i2s audio output. Just like the picture below.
I've already tried a single codec which is connected to the i2s output using the linux simple-card audio driver. I've made a devicetree entry with the simple-card driver and one tas2552 codec which
is connected to an i2c port on adddress 0x40. This setup is working without any problems. I'm looking for somebody who can tell me how I get this setup with 2 codecs working.
As far as I understand it's not possible with the simple-card driver which connects the Ti codec driver to the i2s stream.
I think one should write a custom asoc machine driver. Or maybe the codec driver has to be changed. My asoc knowledge is very limited so I hope somebody can tell my how to proceed.
Kind regards,
Chris