Part Number: PCM4201
Dear TI
I'm debugging PCM4201 because audio noise.
1. System block
2. Mode setting(Master or Slave)
- We are using 11.025KHz sampling frequency.
- Which mode(Master or slave) can be set?
> Slave: 256fs or 512fs
> Master: 512fs
2. About Frame
- Currently, 1 frame was 126BCK not 128BCK. How can I modify?
- We set Normal Speed, high performance mode. Is it same as below "BCK = 128fS when Normal Speed, Low Power sampling"?
> If BCK = 128fS when Normal Speed, Low Power sampling is enabled, then the frame will begin on the falling edge of the FSYNC clock input.
The FSYNC clock is inverted for this case.
- Can you explain High performance mode and Low power mode in Normal speed?
3. Frame sync
- Data is observed previous FSYNC. Is it OK? I think applied BCK delay.
How about your opinion?
4. Not matched One frame size.
- One Frame = 1/Fs = 128BCK(Normal mode)
> 1 Frame = 1/Fs = 1/11.025KHz = 90.7029us
> 128BCK = 128 * 0.354 = 45.312us(waveform 45.30us) --> Not matched
- Is it OK?
5. System Clock
Current system clock: 11.11MHz
Master mode – Normal speed: 512fs = 512 * 11.025KHz = 5.6448MHz -> Not matched
Is it OK?
Please help me.
We cannot next design step because this issue.
Best regards
Lonnie Kim