Part Number: LM48511
Hi Team,
Please help check if the circuit needs adjustment.
1. Condition Vin 5V Output 4 ohm 3W~3.5W
2. Is the circuit part value correct?
3. As shown below
thanks
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM48511
Hi Team,
Please help check if the circuit needs adjustment.
1. Condition Vin 5V Output 4 ohm 3W~3.5W
2. Is the circuit part value correct?
3. As shown below
thanks
Kevin
Hi, Kevin,
The schematic is correct. However, the component values in the schematic will reach more than 3W in this case. For a 4ohms load, you will reach around 5.4-6.7W. Please take a look at the electrical characteristics section below for details (the section 6.5 contains the parameters under the same conditions of the schematic that you attached).
http://www.ti.com/lit/ds/symlink/lm48511.pdf#page=6
If you are looking for a lower output power level, I would recommend to replace the resistors R1393 and R1394 for 10K resistors. These resistors will result in a unity gain (Av = 1) instead of the double (Av = 2). The output power will be then 2.7W to 3.35W.
Please let me know if you have questions or comments on this.
Best regards,
Luis Fernando Rodríguez S.