Part Number: TAS5704
Hello,
Is it possible to request for the ESD values of this device?
It is mentioned in the datasheet that these devices have limited built-in ESD protection, but it seems there is no information on the exact values.
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TAS5704
Hello,
Is it possible to request for the ESD values of this device?
It is mentioned in the datasheet that these devices have limited built-in ESD protection, but it seems there is no information on the exact values.
Thank you!
This is an old device so I'll need to look internally to find this information. I will try to give some information by next week.
Best Regards,
Luis
Hello Elisha
Here are the ESD Ratings for TAS5704
|
ESD - HBM(Human Body Model) |
2000 V |
|
ESD - MM(Machine Model) |
150 V |
|
ESD - CDM(Charge Device Model) |
1000 V |
However I would note if you are making a new design we would recommend the TAS5760.
Best regards,
Luis